Title

Intente buscar por palabras clave, código de producto/pedido o número de serie, por ejemplo, "CM442" o "información técnica"
Introduzca por lo menos 2 caracteres para iniciar la búsqueda.
  • Historial
From linear to circular

Moving from linear consumption to circular value

Traditional linear models follow a "take, make, dispose" approach. Circular economy principles seek to retain the value of materials and resources for longer through efficient use, reuse, recovery and closed-loop approaches.

For manufacturers, this requires considering resource use throughout the lifecycle, from raw materials and production to reuse and recovery.

Productive use of resources

Keeping resources in productive use

Circular manufacturing starts with understanding how resources move through processes and where value can be retained. More efficient production, longer lifecycles and the reuse of suitable materials and process outputs can help reduce dependence on virgin resources while supporting more resilient operations.

  • Use resources efficiently: Identify unnecessary material, water and energy losses and improve the efficiency of industrial processes
  • Extend useful life: Support approaches that keep products, components and assets in productive use for longer.
  • Recover and recirculate: Return suitable materials, water and process outputs to production or other productive uses.
Circular economy wheel: From product design and production to recycling ©Endress+Hauser
Processes & value chains

Circular manufacturing connects processes and value chains

Circularity often extends beyond an individual process or facility. Secondary materials, reusable process outputs and recovered resources can move between processes, sites and organizations.

Closed-loop approaches and collaboration across value chains can create opportunities to retain resource value and reduce demand for additional raw materials. Reliable information about the quality, quantity and characteristics of these resources can support decisions about their potential reuse.

Water reuse

Keep water in circulation

Treating and reusing water can reduce demand for freshwater resources, reduce dependencies and support more resilient industrial water cycles.

Tratamiento avanzado de aguas residuales para su reutilización

El aumento de la reutilización del agua se apoya en metodologías de tratamiento avanzadas, innovadoras, seguras y cada vez más rentables. 

Más información

Abordar el panorama normativo de la reutilización del agua

Abordar los desafíos internacionales relacionados con el agua requiere marcos normativos seguros que adopten soluciones de reutilización del agua innovadoras.

Más información

Gestión de los riesgos de la reutilización del agua

La reutilización directa e indirecta del agua potable son prácticas conocidas, pero es fundamental conocer los riesgos asociados para proteger la salud humana y el medio ambiente.

Más información

Gestión de los riesgos de la reutilización del agua

La reutilización directa e indirecta del agua potable son prácticas conocidas, pero es fundamental conocer los riesgos asociados para proteger la salud humana y el medio ambiente.

Más información

Filtración por membrana para garantizar la calidad del agua

La instrumentación de proceso desempeña un papel crucial en la filtración por membrana para garantizar la máxima calidad del agua. El reto operativo radica en prevenir la suciedad, la obstrucción y el deterioro de las membranas.

Más información

Circular and bio-based resources

Create value from alternative resources

Biocombustibles sostenibles: ampliación de la escala para una economía circular eficiente

Descubra cómo los biocombustibles sostenibles transforman materias primas renovables y corrientes de residuos en valor, impulsando los objetivos de economía circular, la reducción de carbono y la eficiencia en el uso de recursos.

Más información

Productos bioquímicos y economía circular: cómo optimizar la cadena de valor biotecnológica

Conozca los factores clave, las presiones regulatorias y los desafíos operativos que están dando forma a la cadena de valor biotecnológica en la producción de productos bioquímicos

Más información

Producción de biogás y biometano a partir de lodos y residuos

De los residuos a fuentes de energía aprovechables: descubra cómo la producción de biogás y biometano combina la digestión, el enriquecimiento y un funcionamiento estable para favorecer la gestión circular de los recursos.

Más información

Waste management

Recover value from unavoidable waste

Preventing waste and keeping resources in productive use remain central to a circular economy. When waste cannot be avoided or directly reused, effective waste management can help recover remaining material or energy value and manage residual materials responsibly.

Waste management therefore complements circular economy strategies by addressing resources once prevention and direct reuse are no longer possible.

Procesos y tecnologías de gestión de residuos que impulsan mejoras en la economía circular

La gestión eficiente de los residuos es esencial para garantizar la sostenibilidad, el cumplimiento de la normativa y el éxito empresarial.

Más información

La incineración de residuos convierte los residuos no reciclables en energía fiable

El tratamiento térmico de residuos desempeña un papel clave en la gestión moderna, ya que reduce de forma significativa su volumen, produce energía renovable fiable y elimina contaminantes del ciclo de nutrientes.

Más información

Process transparency

Measurement brings transparency to circular processes

Circular improvements depend on knowing how resources move through production. Reliable measurement and process data help provide visibility into inputs, outputs and losses and identify where resources can be used more efficiently. This transparency can support manufacturers in:

  • Identifying resource losses and efficiency opportunities
  • Monitoring material and resource flows
  • Optimizing processes for reuse and recovery
  • Evaluating improvements using reliable operational data

Measurement therefore connects circular economy ambitions with day-to-day industrial operations.

Measurable progress

Turn circular ambitions into measurable progress

Circular economy initiatives become more actionable when resource flows and improvements are transparent. Relevant indicators depend on the process and application and can include resource consumption, material losses, secondary inputs, recovered outputs and water or energy use.

  • Understand resource flows: Establish transparency around resource inputs, outputs and losses.
  • Improve resource efficiency: Identify opportunities to reduce consumption, prevent losses and increase reuse or recovery.
  • Verify progress: Use reliable operational data to understand whether improvements are delivering the intended results.

Building a more circular industrial future

The transition toward a circular economy goes beyond better end-of-life management. It starts with using resources efficiently, preventing unnecessary losses and identifying opportunities to keep materials, water and other resources in productive use.

Reliable measurement, efficient processes and collaboration across value chains can help manufacturers turn circular economy principles into practical improvements and strengthen resource resilience.

FAQ

Everything you need to know about circular economy in process industries and manufacturing

Notas al pie

Looking for more?